10/17/2018 7:47 AM | |
Posts: 35 Rating: (1) |
Dear all, please anybody can tell me what is HIGH SPEED COUNTERS (HSC) in S7-1200 plc???? also tell use of it..... |
10/17/2018 12:22 PM | |
Posts: 2826 Rating: (685) |
Hello Sharon Joy. Added is a rough definition, which is now redundant with all the fine answers already given. There are important information in the manual of the PLC that is essential reading for clearing up specific details. Notice also that there are big differences between the generations of processors. A more detailed description of what you have, might be followed with application specific hints. Regards. AttachmentHSC.txt (383 Downloads) |
Follow us on