(3)| 8/21/2010 3:43 PM | |
|
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Muhammad, You have a problem with your Analog Card at Address 224. As you see in the below report from the Diagnostic Buffer: 1.Line 5, there is a ADC/DAC error which is referring to Analog to Digital conversion in the Card. 2. Line 9, there is an External Error which referring to the cause of the error from outside of CPU. I recommend you to replace the Analog Card with a spare one. Regards, Behnam www.sigmaprocess.ca/blog ------- Event 2 of 100: Event ID 16# 3842 Module OK Module type: Analog SM Input address: 224 ADC/DAC error Channel information available Requested OB: Diagnostic interrupt OB (OB82) Priority class: 26 External error, Outgoing event 09:03:50.120 AM 11/27/2000 -------- |
Follow us on