12/13/2017 9:56 AM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating: (39) |
Hello everyone. Currently don't have opportunity to check this (see attachment) on real hardware. Most interesting is that it worked initially fine, once after creating a project, hardware config and so forth. But, once I added NW3, for example, to use T1, T2 itself or M1.0 or M1.1 further in the project. I've got it freezed as it showed in attachment. Well, I deleted NW3 , did download again, but it's still refusing to run. if I'll create a new project with two NWs. Then there will no problem there. That will run fine again until I create NW3 and use signals from NW1,2. So it is going to be unuseful thing as I cannot utilize it further in the sample project. Please any comments! Msorich Attachmenttest_two_timers.pdf (27 Downloads) |
12/14/2017 9:07 AM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147) |
Hello, Can you give some information about the Software you are using? Which versions exactly? Best regards, Wizard |
12/14/2017 11:00 AM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating: (39) |
SM itself V5.5 SP4 HF11; PLCSIM V5.4 SP5 Upd2; Msorich |
12/14/2017 11:09 AM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147) |
Hello, Perhaps you can use the latest Service Pack: Trial Software SIMATIC S7-PLCSIM V5.4 SP8 Best regards, Wizard |
Follow us on