7/21/2018 1:16 PM | |
Posts: 35 Rating: (1) |
dear all, plz tell me what is the difference between 1vpp and ttl in encoder which can be used in SMC20 and SMC30 SENSOR MODULE. |
7/21/2018 1:45 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello, Encoders whose output signal waveform is sinusoidal in nature & amplitude value is 1Vpp are called as 1Vpp. Where as encoders whose output signal waveform is square wave is called as TTL (Transitor Transistor logic), its output is 5 or 24 V depending upon supply voltage. SMC20 - Incremental encoders with sinewave 1 Vpp output are connected to SMC 20. SMC 30 - Incremental encoders with TTL or HTL output are connected to SMC 30. Please refer attachment for more details. AttachmentSMC 20 & SMC 30 .zip (389 Downloads) |
This contribution was helpful to1 thankful Users |
7/21/2018 1:58 PM | |
Posts: 35 Rating: (1) |
THANK YOU SO MUCH SIR. |
1/21/2021 9:36 PM | |
Posts: 1 Rating: (0) |
Osea no puedo conectar un codificador 1Vpp al SMC30? |
Follow us on