7/21/2018 5:34 PM | |
Joined: 8/30/2017 Last visit: 4/1/2024 Posts: 4 Rating: (0) |
Hii, I am in a trouble. I already have 3 ET 200 series CPU; IM 151-8 CPU and 1 s7 300 series CPU 314C-2PN/DP in communication, and I want to add 5th new station, S7 1200 firmware version 4.0 (MLFB no is= 6ES7-215-1HG40-0XB0),but I can't achieve communication between S7 1200 (4.0 firmware) CPU and Wincc v7.2 Runtime. Corrective actions I have taken: 1. Installed Simatic NET PC 8.2 + SP1= Is it correct version or should I install without SP1.?? 2. I have attached IE general in the hardware of the program and given the IP of scada pc to the IE general and downloaded into the S7 1200 CPU. although communication is not happening. So please guide me what next to do to achieve the communication.Here I have also attached some screenshots. Is S7 1200 IP tool necessary for communication.? with regards, Mitul SUthar
Attachmentwinc 7.2 and s71200.zip (105 Downloads) |
Last edited by: ganesha@2512 at: 7/21/2018 5:39:38 PMLast edited by: ganesha@2512 at: 7/21/2018 5:45:43 PM |
|
7/21/2018 6:04 PM | |
Joined: 8/30/2017 Last visit: 4/1/2024 Posts: 4 Rating: (0) |
Hii, I am in a trouble. I already have 3 ET 200 series CPU; IM 151-8 CPU and 1 s7 300 series CPU 314C-2PN/DP in communication, and I want to add 5th new station, S7 1200 firmware version 4.0 (MLFB no is= 6ES7-215-1HG40-0XB0),but I can't achieve communication between S7 1200 (4.0 firmware) CPU and Wincc v7.2 Runtime. Corrective actions I have taken: 1. Installed Simatic NET PC 8.2 + SP1= Is it correct version or should I install without SP1.?? 2. I have attached IE general in the hardware of the program and given the IP of scada pc to the IE general and downloaded into the S7 1200 CPU. although communication is not happening. So please guide me what next to do to achieve the communication.Here I have also attached some screenshots. Is S7 1200 IP tool necessary for communication.? with regards, Mitul SUthar
Attachmentwinc 7.2 and s71200.zip (93 Downloads) |
7/22/2018 8:50 PM | |
Joined: 9/19/2009 Last visit: 5/5/2024 Posts: 458 Rating: (81) |
Hi Sorry about the question... Have you tried to do a ping? Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
7/23/2018 2:15 PM | |
Joined: 9/3/2008 Last visit: 5/8/2024 Posts: 921 Rating: (158) |
Hi, Which update to WinCC do you have installed? You need at least update7 to communicate with 1200 fw 4. |
Michael |
|
7/30/2018 3:26 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (39)
|
Hi, there you can get the newest update: Update13 https://support.industry.siemens.com/cs/ww/de/view/109739416 regards |
Grundkurs/Systemkurs WinCC V7: |
|
7/31/2018 1:50 PM | |
Joined: 2/8/2011 Last visit: 9/7/2023 Posts: 87 Rating: (8) |
Dear All, I saw the same problem and when I search documents in WinCC training I saw a help pdf. I am sending to for all guest that documents. You can see a base way for communication between S7-1200 / 1500 and WinCC. Best regard. Attachment02_02_Communication_S7-1500.pdf (159 Downloads) |
Follow us on