7/21/2018 9:36 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Selection of SLM module involves engineering & difficult to select based on only one specification like total motor current. How many motors will be at rated load at single instance? What is the duty cycle? Have you considered the ambiant conditions? 30 A which is total current of all motors, is it peak or contineous or full load current? However you may refer attached sheets having details of SML specifications & will help you to understand SLM engineering. (It is internal cooling) AttachmentSLM specification & details.pdf (128 Downloads) |
Follow us on