11/13/2018 3:54 AM | |
Posts: 15 Rating: (0) |
Good day everyone, For today, I may need assistance as to why the Current readings in the TIA portal is stagnant when I attempted to read from a targeted Current. I am not sure if its my wiring configuration, the hardware, or my TIA portal is not in order. Here are the details; CPU: ET200SP AI module: AI 8xI 2-/4-wire BA (6ES7134-6GF00-0AA1) Current Transducer: SENECA T201DCH50-LP Attempted flow current through hole: 1.5 A 50 V Phone charger to phone. Output wanted to achieve and shown in TIA portal: Between 4 - 20 mA. My wire configuration is as shown on SS1 (Attached). Supply current to Current transducer from PLC is at 24 DC 10 A. My block diagram and tag table as shown on SS2 and SS3. Currently test_1 (%IW0) is the only channel I activated. The others are deactivated and result in the value 32767. Switching on and off flow current result in no change of value. E.g. between 45 to 55 for test_1 . I gotten the block diagram from youtube, in which in any case, I believe %IW0 would result in some value. My device configuration as at TIA portal as shown on SS4.1 and SS4.2. Wiring are according to 2-wire connection. What do I do wrong? :( Looking foward for your reply. Connecting Current Transducer into AI 8xI 2-/4- wire BA
AttachmentSS.zip (230 Downloads) |
11/28/2018 8:21 AM | |
Posts: 15 Rating: (0) |
Thank you CaOd. Now I got the essence of the CT and its connection. Will be moving on to my next question. |
Follow us on