8/17/2018 6:20 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
Hello, is not possible to get this information from the panel . Why you need this Information? Regards Christoph |
8/17/2018 11:05 AM | |
Joined: 9/21/2012 Last visit: 9/20/2024 Posts: 4148 Rating: (464) |
If you want to do a backup, use ProSave software. |
Last edited by: Jen_Moderator at: 8/17/2018 11:10:18 AMOptimized link. |
|
8/17/2018 11:26 AM | |
Joined: 7/27/2018 Last visit: 8/14/2023 Posts: 13 Rating: (0) |
Hello Hati, I tried to back up by Prosave but could not. I'm with TIA V13, WinCC Flexible 2008 V1.3, STEP 7 V5.5 installed on a VM Virtualbox. When I open Prosave I realize it's in version 13, I think it's because it's with TIA V13 installed. Can I back up this panel by having Prosave in V13 installed?
|
8/17/2018 11:32 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
Hello, yes should be possible with this ProSave Version.
Christoph |
Follow us on