8/18/2018 11:07 AM | |
Joined: 1/1/2017 Last visit: 7/22/2024 Posts: 331 Rating: (11) |
Dear All, Presently I'm facing a problem in Step 7 regarding one DO address. The address is Q21.6. The address is used twice in the logic, once in OB1 & the other in FB 13. Problem is that when I'm giving command from HMI the output is getting high in logic but the field address in DO module is remaining in low state. I'm simply horrified with this problem & didn't knew how to tackle with this issue. Please help me as the problem is still unknown to the Client. Regards OmKris AttachmentCoal_Stacker_18082018_1127.zip (41 Downloads) |
Follow us on