10/18/2018 12:18 AM | |
Posts: 4 Rating: (0) |
Hi, I just downloaded PST V4.+ HF1 on windows 10 64-bit. We are trying to set the IP address on SCALANCE access point and client devices. The problem is when I try to browse then PST prompts "Error 2:1 Please select a suitable interface parameter assignment..." Then when I go to Settings > Set PG/PC Interface, nothing shows up. So the goal is to change the IP address over Ethernet. Grateful for any advice, thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/18/2018 10:44:08 AMNew subject after splitting |
|
10/18/2018 4:27 PM | |
Joined: 8/3/2009 Last visit: 9/19/2024 Posts: 13742 Rating: (1730) |
Hello qrd You could also use Proneta instead of PST: https://support.industry.siemens.com/cs/ww/en/view/67460624 Bye Murof |
If this Information really helps, you could use the Rate function |
|
12/23/2019 10:01 AM | |
Posts: 1 Rating: (0) |
Exactly same is happening with me. No devices to select! |
Follow us on