11/20/2018 5:54 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Bhairava, I have two suggestions here. 1. May be you could try check whether your CFC version is the latest one? Software Updates 2. Try update your block contacts, make sure the block contact in sfc is the latest one? see attached pictures. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
11/20/2018 10:41 AM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927)
|
Can you check if the Vlvl block in the blocks folder and project folder have the same attributes? Maybe an attribute s7_contact is missing in your project folder? And the update of cfc software is a must. Since the use of CMT in PCS7 , Siemens has released a lot of updates. My thoughts are that they do not control the CMT perfectly . Issues are still being solved . So updating is your best bet.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on