12/18/2018 10:52 AM | |
Joined: 7/12/2018 Last visit: 11/25/2023 Posts: 1 Rating: (0) |
please how to solve this problem posted below ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/18/2018 1:51:56 PMNew subject after splitting |
|
12/18/2018 2:22 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, The block is using a FC that is not in the valid range. To solve this, do as follows: In CFC go to Options->Customize->Compile/Download. Under Areas reserved for Other Applications, you can adjust the FC range so that the FC falls within the limits. that is one option, the other one is to determine the FC and see if you can rename it in your project, but for FC's used by the system, it should not be done. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on