12/4/2018 10:13 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see attached screenshot. I am making 2 flexpanels to show gear positions. The position of these gears are already shown on the main HMI panel which is which is connected to a WinCC 7.4 server. I need to show the same on the flexpanels (one panel for SG1 and one for SG2) as is shown on the main HMI screen. in WinCC 7.4 a faceplate (DigMonitor.fpt) is used to show different colors (grey, white, red and green) depending of the value of the connected DBW. Since I cannot use the faceplate in the flexpanels I need to do it a little differently there. I CAN however make a square be different colors for different values. So - how do I see which DBW value corresponds to which color in the WinCC 7.4 faceplate? I have used VAT's to see the values (as decimal numbers) of the current position so it looks like 18 is green and 32 is grey - but which number is white and which is red? (and also it seems 26 might be green also on 2 occasions). I am not allowed to just move the gear levers as I would like to get the missing indication on the main HMI screen. AttachmentFlx34.zip (36 Downloads) |
12/6/2018 7:43 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Sure some of the smart members here can advice me on this? |
12/18/2018 11:04 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
By using PLC-SIM and OS Simulation I managed to see what I needed :-) |
Follow us on