2/16/2019 6:15 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33799 Rating: (4199)
|
If you correct the block name error (I have overlooked it despite multiple searches), the program still can not be converted to a 0BA6 program (as noted by Scorp, thanks). The strange thing is that he complains about an OR block B201, where there are no OR blocks in LAD. And there is also no block in LAD called "Bxxx". If you convert the program to FBD, you will find this (and other) OR block. From B201 there are different OR or AND blocks in FBD. And since the 0BA6 has only 200 blocks, you can not convert this program to a 0BA6 program. If you replace the blocks with the numbers greater than 200 in FBD against blocks with a smaller number, so that no block number greater than 200 exists, you can select a 0BA6 as a device and convert the program back to LAD. It can be concluded: LAD at the LOGO! is a bad, error-prone implementation of the programming language FBD of LOGO !. AttachmentLXL VFD 4.0 for 0BA6 for forumguy_0BA6.zip (283 Downloads) |
Last edited by: ixo65 at: 2/16/2019 6:17:17 PM |
|
This contribution was helpful to2 thankful Users |
2/16/2019 7:32 PM | |
Joined: 10/20/2015 Last visit: 7/13/2024 Posts: 94 Rating: (19) |
Hahaha... you are right. And I agree, for the LOGO! the programming language is FOR SURE FBD! |
2/19/2019 3:35 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33799 Rating: (4199)
|
There's a first time for everything.... |
Follow us on