2/5/2017 6:34 PM | |
Posts: 623 Rating:
|
Hi Cheese11, Data block comparison- In the first step of the process, STEP 7 compares the time stamps for the interfaces of the data blocks to be compared(as for logic blocks). If these time stamps are identical, STEP 7 assumes that the data structures are identical. If the interface time stamps are different, STEP 7 then compares the data structures until the first difference is found. If the data structures are in the sections are identical, STEP 7 then compares the initial values and current values. All differences are displayed. U can use Go to button to see actual differences between these 2 DBs. |
This contribution was helpful to
1 thankful Users |
Follow us on