7/30/2017 2:54 PM | |
Posts: 4 Rating: (0) |
after reading several posts on this forum I have a few more questions about the axis information. the drive that alarmed out due to overtemp on the heatsink is the drive that controls the two rotary axis on the machine. the linear axis did not alarm out. I am dealing with an MMC100 and just PCIN loaded in a laptop. the original PCU that came with the machine is long gone. how can I be sure that the drive information is correct. and how can I change the parameters if it is indeed incorrect. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/31/2017 10:41:29 AMNew subject after splitting |
|
7/31/2017 10:42 PM | |
Posts: 4 Rating: (0) |
I have none of these things |
Follow us on