2/29/2016 12:08 PM | |
Posts: 62 Rating: (0) |
[snip] Ok i have another questions abaout X ax (vertical ax) on turning maschien. When i driving this axe in minus or plus direction motor giving annoying voice? On this axe we have auxiliary cylinder. When the axe is staying on one position the current is jumping from 5 to -12 A and speed actual value is jumping from -21 to 16RPM? is this ok or not? Thank you again for your help ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/1/2016 10:24:38 AMNew subject after splitting |
|
2/29/2016 1:06 PM | |
Posts: 62 Rating: (0) |
So if my motor of x axis gives strange annoying sounds it,s not a problem, and i cant damage a motor? |
3/1/2016 10:41 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please try again by reducing it go upto 0.3 value. Your motor brake is OK as the motor current is within limit (mentioned by you in earlier post.) Have you checked vertical axis lubrication? Is it ok? How many measuring feedback systems are installed for vertical axis? |
Follow us on