11/14/2010 9:25 AM | |
Posts: 69 Rating: (1) |
DEAR SIR, I AM USING ABSOLUTE ROTARY ENCODER (MAKE:HEIDENHAIN) FOR Z AXIS IN SIEMENS 840D SYSTEM.REFERENCE SYSBOL SHOWING AND PARAMETER 34210 SHOWING 2. BUT AFTER POWER ON AND OFF, MACHINE VALVE SET TO ZERO REFERENCE LOST. HERE WITH I ATTACHED NC.ARC FILE PLEASE KINDLY HELP ME TO SOLVE THE PROBLEM. SYSTEM:840D NCU: 572.5 HMI:6.4 ROTARY ENCODER DETAILS ************************************** MAKE: HEIDENHAIN ROC 413 RESOLUTION :2048 AttachmentNC2510.zip (374 Downloads) |
11/17/2010 9:00 AM | |
Posts: 69 Rating: (1) |
Dear Sir, Thanks for your reply, As per your instruction all the external encoder parameter has been set correctly.In that machine there is 6 axis and one spindle , all are absolute encoders. I having problem with z and A axis only.reference position lost after every time power off and on. other X , Y, W, B axes are working perfectly. here with i attach nc archive file in pdf format, Kindly help me to slove the problem. AttachmentNC_17_11_2010.pdf (529 Downloads) |
11/18/2010 5:19 PM | |
Posts: 69 Rating: (1) |
Mr. Ekalavya, Thanks for your reply, all my motor encoder are absolute enocders. if I enabe motor encoder for Z and A axis Absolute encoder did not lost reference position and working properly. If I enable external encoder , reference postion lost every time power off and on time. In that Machine there is 6 axes and one spindle, X, Y, Y, W , B, SP, A. X,Y,W axes are external encoder enabled - heidenhain Linear scale absolute. B, A, Z axes are external encoder enabled - heidenhain, EnDat01, 2048ppr. Kindly help me to slove the problem. External Encoder details ****************************** Make : Heidenhain model : ROC 413 EnDat01 Resolution : 2048 regards, Balaji AttachmentNC_17_11_2010.pdf (231 Downloads) |
11/19/2010 2:35 PM | |
Joined: 6/7/2010 Last visit: 2/3/2023 Posts: 569 Rating: (37) |
Hi ganesh, Could you send me the PLC backup |
Regards, |
|
11/21/2010 2:57 PM | |
Posts: 69 Rating: (1) |
Hi Experts, Herewith i attached PLC backup, Regarding Absolute external rotary encoder position lost, every time power off and on in 840 D system. I changed external Z axis encoder cable after there is no improvement. If i set 36310 ENC_ZERO_MONITORING bit in Z axis and try to move the axis. Then alarm 25020 Axis Z zero mark monitoring of active encoder came. Please help me slove the problem. AttachmentWotan__Boring.zip (297 Downloads) |
Follow us on