6/25/2015 6:46 PM | |
Posts: 2 Rating: (0) |
hello I just need to backup PLC on the hard drive or I need to make a copy in a diskette or usb? thanks in advance
|
Last edited by: Min_Moderator at: 6/26/2015 10:12:40 AMNew subject after splitting |
|
6/26/2015 2:19 PM | |
Posts: 110 Rating: (3) |
Hi ITS MEXICO what is type of control and which version Ali Rana |
1/15/2016 5:39 AM | |
Joined: 6/23/2009 Last visit: 7/15/2024 Posts: 22 Rating: (0) |
It's been a long time ago but now I'm facing this task, used the SinucomNC connecting to NCU and do the "Create Archive" with NC and PLC selected. Now I have the *.arc file (which is attached to this post also) stored on my computer. Is it enough if I get the NCU replaced and then restore this backup? Does the NC section of this backup has all Simodrive 611 digital's parameters and settings? How can I do the restore because there's no "Download" or "Restore" button...
AttachmentSinumerik_840D_PL.rar (689 Downloads) |
huytai.tran@gmail.com |
|
1/18/2016 1:17 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, 1. PCU hard disk clone image you can use as back up of particular machine & is useful in case when the user needs to reload the back up. User can not use the clone back up for any another type of machine or as software backup. 2. It depends upon how you are purchasing PCMCIA card (It is not NCU, please note NC card & NCU card are different. NC card is PCMCIA card which has got system s/w, where as NCU card is with processor, memory BIOS system etc) i.e. with system s/w or w/o system software. When back up is taken on PCMCIA card, user cannot access it, moreover PCMCIA card needs cardware s/w to copy or back up data on another PCMCIA card. Where as if user took back up of NC, PLC or series start up data on PC, user can access different data files. (Its possible when when Data, start up data, etc or NC, PLC data in .arc files is taken. Please take NC with compensation & PLC data backup separately.) Please note, when restoring back up data on NCU, NC, PLC data needs to be cleared. Please go thru the attached files, for more information. Please take atmost care while clearing data unless & until you are sure that you have correct backup data & of correct machine. :-) HTH Attachment810D data bck up restore 1 .zip (649 Downloads) |
Last edited by: PISCEAN 2010 at: 1/18/2016 1:17:54 PMFile 1 added Last edited by: PISCEAN 2010 at: 1/18/2016 1:22:18 PMLast edited by: PISCEAN 2010 at: 1/18/2016 1:31:15 PM |
|
This contribution was helpful to3 thankful Users |
1/18/2016 1:19 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
File 2 attached
Attachment840 D data bck up restore 2.zip (612 Downloads) |
Last edited by: PISCEAN 2010 at: 1/18/2016 1:23:00 PM |
|
This contribution was helpful to2 thankful Users |
Follow us on