7/2/2013 10:45 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839)
|
Hello, Hope this helps.
|
Ayman Elotaify |
|
7/3/2013 9:18 AM | |
Posts: 139 Rating: (5) |
Hello@shish, Thanks for reply. Can read out LED states ald? the reason why i asking is i did reading for all 13 LED states for H-CPU by using SFC 51 with own code. and if you are using H-CPU and not solved yet, i can help with some time.
|
7/5/2013 7:53 AM | |
Joined: 9/16/2011 Last visit: 6/20/2024 Posts: 291 Rating: (6) |
Dearhdhosseini, I have used your sample program that you have sent me, but i am getting the value at RET_VAL is 8085 with SSL_ID w#16#0119 which states that "Due to a problem in the system, information is not currently available" kindly suggest ! Reg, Ashish
|
Reg, |
|
7/5/2013 8:00 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello, The program was not my sample, it is an example available here and just give you the correct link.About your problem, as far as comments in networks #2 and #3 suggest, CPU first check the SSL 0119 and in case of error switch to SSL 0174.Check the comment and see the RET_VAL in block called in network #3. Best regards Hamid Hosseini |
7/5/2013 8:11 AM | |
Joined: 9/16/2011 Last visit: 6/20/2024 Posts: 291 Rating: (6) |
Dearhdhosseini, I guessed you are the expert and wrote such beautiful program for me. well, coming to the program, in network-2 i am getting RET_VAL 8085 (-32635) and network-3 is not being executed.
|
Reg, |
|
7/5/2013 8:21 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello again, I have written several codes in STL and SCL here, I never try LAD,You can search for what I have done here.In what CPU are you checking the program?The feedback from the block should be like this: 8082 SSL_ID is wrong or is unknown in the CPU or SFC. (-32638) in your case, I guess you are trying execution on PLCSIM? 8085 Due to a problem in the system, information is not currently available (for example, due to a lack of resources). (-32635) Update for more information Hamid Hosseini |
Last edited by: hdhosseini at: 7/5/2013 8:28 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on