6/4/2010 5:16 PM | |
Posts: 2964 Rating: (478) |
Hello... When Hardisk is totally deffective you want to replace with the new one following activity to be done 1. Emergency boot diskettes- all 3 floppys to be extraced in DOSfor getting SERVICE Menu screen, 2. Make proper Ghost connections parameter. 3. Restore the Ghost Image to restored back. EMERGENCY backup image can be taken when machine is healthy condition. I am attaching you document which present in DOCON WEB When Emergency Backup image is Restored in the Harddisk only Windows Base get loaded but you should keep the local partition image in the hard disk for restoring the other drives(C,D,F) I Would suggest to take the whole Ghost Image backup keep it CD/hardisk and Local Partition Image in the harddisk. For Emergency Boot diskette openyour GHOST image file with Ghost explorer and check for the same. hope this will help your requirement... bye/Ekalavya AttachmentEmergency Backup image.pdf (197 Downloads) |
6/4/2010 5:48 PM | |
Joined: 10/17/2007 Last visit: 4/22/2024 Posts: 3972 Rating: (340) |
Thanks Ekaiavya, It is very helpfull. |
If you like my comments please |
|
6/5/2010 10:49 AM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating: (176)
|
Hi >Conezilla live USB I think you mean "Clonezilla live USB" |
Karl |
|
6/5/2010 5:30 PM | |
Posts: 259 Rating: (5) |
Thats right. Wrong spelling. But the most important thing: You understood me.:) Makaveli |
6/6/2010 10:42 AM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating: (176)
|
Hi Logically |
Karl |
|
Follow us on