8/5/2019 3:36 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Check out this thread to see how you can achieve that over an S7-Connection. Kind regards! |
This contribution was helpful to1 thankful Users |
8/8/2019 12:37 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, You can select node-red to run and startup in:
Node-Red has a web-interface, so its accessible over the browser. By the way there are various ways you could communicate with the S7-1200... You could also use Modbus-TCP or TCP directly with TSEND TRCV. And you don't necessarily have to use node-red, its just the easiest way. You could also use python, C++ or native NodeJS. Kind regards! |
Last edited by: Fe_lipe at: 08/12/2019 15:26:00updated link |
|
8/9/2019 6:57 AM | |
Posts: 12 Rating: (0) |
Hi Fe_lipe, Thank you for your recommendation, I think I will work in to TCP directly and use python to develop script. There are several samples in the internet for python snap7.
|
Follow us on