8/5/2019 6:17 PM | |
Joined: 5/15/2015 Last visit: 12/16/2023 Posts: 9 Rating: (0) |
Hello. In one of the controllers (941), the PG connector is faulty. There is a spare controller (942) with a power supply. The battery is bad, the LED is on. There are I / O modules on the mounting rack (not like in 941). He turned on 942, did the erasing of the memory, took eprom it out of 941, inserted it into 942. Turned it on - the RUN lights up in green, there are no red ones. But there is still no connection with PG. As if he didn’t “see” the eprom with the program. Maybe I'm doing something wrong? Or 942 is also faulty. (communication adapter is working). ------------------------------------------------------------------------------------------ |
Last edited by: nicss at: 08/05/2019 18:20:45Last edited by: nicss at: 08/05/2019 18:29:07Last edited by: Jen_Moderator at: 08/06/2019 09:19:58New subject after splitting |
|
8/6/2019 6:43 AM | |
Joined: 5/6/2010 Last visit: 4/17/2024 Posts: 1963 Rating: (271) |
Hello nicss, you have the "problem" that you use not a really adapter. You use a cable and no more. The challenge is that you need a serial interface which can TTY (current loop). A "normal" RS232 doesn't work . You need a active RS232 and a adapter from RS232 to TTY. You can use e.g. (german website) IBH USB-S5-Adapter or ACCON-COM-Cablel USB regards |
8/9/2019 12:52 PM | |
Posts: 68 Rating: (1) |
Hello nicss, S5 cpu (941/942) transfer the Program Two way Possible. 1.Through EPROM transfer the program. 2.Upload Proram from 941 controller and Down load to 942 controller. Required Document attached here.Any Clarification Msg me. AttachmentS5 941 EPROM Program transfers .pdf (140 Downloads) |
8/9/2019 12:55 PM | |
Posts: 68 Rating: (1) |
Hello nicss, S5 upload the programs from CPU. Please find the attachment. AttachmentS5Upload.pdf (132 Downloads) |
8/20/2019 8:11 PM | |
Joined: 5/15/2015 Last visit: 12/16/2023 Posts: 9 Rating: (0) |
This board was to blame. Restored and it worked. Thanks to everyone. |
Follow us on