7/16/2016 7:12 AM | |
Posts: 92 Rating: (5) |
Hi there im work on a Sinumerik 810T GA2 and PCIN on Windows XP in PC Im also online and my cpu type is :150U my Backups file all is as a ".txt" f.e : PCP.txt PCA.txt TA1.txt and ... Bout rate in PCIN,COM por setting,Sinumerik810 :300 Or 11000010 5010/5012 :00000000 5011/5013 : 11000010 5016 : 00101000 I set my cable like this,with sheald and earth protection: 9 PIN 25 PIN 1--------1 sheeld 2--------2 3--------3 4--------6 5--------7 6--------20 7--------5 8--------4 same as the pcin comment. To be sure as The whole memory is erased , i remove my battery after that start to inittial. I can Download %TEA1 and %TEA2 as well as,But when i want to Download %PCP ,after 1800 Byte,DIO will disappear and transfer will be stopped. Also i can Download other Machins %PCP to this system control , its work as well as! But system controls own %PCP ,Not. I've been Try Many things with diferent cable's,but same result. I'm suspicious to this : At the friest,I Do step by step any thing in reload pdf file,but after second reset(after Download TEA1 and TEA2 ) I need to press "END stup PW" and Press diagnosis,then Eyeball, pasword-->enter But when I press Inittial clear mode ,its show : NO Key-Operated Switch Here is photo so i have to hold Eyeball agein and go to Initiall clear mode
thanks a lot for your attention Best regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/18/2016 12:39:18 PMNew subject after splitting Last edited by: Sky Diver840 at: 8/2/2016 8:58:45 AM |
|
7/28/2016 11:40 AM | |
Posts: 92 Rating: (5) |
I Attached Files And Picture of "NC ALARM " And transfering %PCP. And Here is Alarms Too: [ NC ALM : 3 ORD 1 Plc stop Alarm message from NC 3 ORD 1 Plc stop 2153 ORD 2 control loop Spindle - HW ] [ PLC ALM : 3 ORD 1 PLC STOP Alarm message from plc 6127 alarm byte messing ] [ PLC MESSAGE :
PLC MESSAGE ] AttachmentPic Of ALA & PCP TRNSFR.zip (497 Downloads) |
7/31/2016 7:19 AM | |
Posts: 92 Rating: (5) |
here is attached first four page of PCP program display and the last page too. yes,I have step5 V7.2 , I'm Online and also can DOW/UPLOD sample files. I have not 6127 ALM on system control after reload TEA1 and TEA2 and PCP,after reload TEA1 and TEA2 , I just have PLC stop Alarm. transfer part by part and check the alarms, to find wich file is responsable of "Messing Byte Alarm" ,is this right? AttachmentPic.zip (263 Downloads) |
Last edited by: Sky Diver840 at: 8/1/2016 5:38:25 AM |
|
8/10/2016 7:38 AM | |
Posts: 92 Rating: (5) |
Hi there after trying and hard exploring , I can finde " HandBook of Wiring diagrams " Of my machine. In this book i have [ block listBlock type And OB, PB , FB too. I have step5 and is it possible to I rewrite it from base ? can you help me please dear adventurs? My %PCP and %ASM are corrupted. AttachmentDesktop.zip (285 Downloads) |
8/15/2016 4:04 PM | |
Posts: 1 Rating: (0) |
Hi! It would be necessary to help! Sinumerik 810T PC software should be German, in English for now. Thanks!
|
8/17/2016 6:54 AM | |
Posts: 92 Rating: (5) |
Finaly I finish it My both 810T Works as well as and It was Unpossible Without Your Kindly Help. thank you , Mr Pee, Mr Nulizhng Mersi ( "mersi" is thank in my org language) I had [ PLC ALARM MESSEGE 6127 and ORD1 PLC STOP ], as you know it means is : " Selected interrupt input byte not available in hardware After error and trail I find its work in 15 and because i had new alarm 6104 ( Parameterization error in BMW or BDW command so I just chenge bit 0 to 1, in MD2002 . Orginaly it was : 10101000 and i chenge it to : 10101001 . Its work and my PLC STOP ALM cleard. I jast want to Know , Is it ok? Its work know but in future or in work it didnt make misstake? MD2002 Bit 0 is : [ No PLC alarm processing [ explanation PLC-MD 0
Attachment338_810_820_GA3_Installation_Instructions.pdf (352 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on