7/31/2016 7:19 AM | |
Posts: 92 Rating: (5) |
here is attached first four page of PCP program display and the last page too. yes,I have step5 V7.2 , I'm Online and also can DOW/UPLOD sample files. I have not 6127 ALM on system control after reload TEA1 and TEA2 and PCP,after reload TEA1 and TEA2 , I just have PLC stop Alarm. transfer part by part and check the alarms, to find wich file is responsable of "Messing Byte Alarm" ,is this right? AttachmentPic.zip (262 Downloads) |
Last edited by: Sky Diver840 at: 8/1/2016 5:38:25 AM |
|
8/10/2016 7:38 AM | |
Posts: 92 Rating: (5) |
Hi there after trying and hard exploring , I can finde " HandBook of Wiring diagrams " Of my machine. In this book i have [ block listBlock type And OB, PB , FB too. I have step5 and is it possible to I rewrite it from base ? can you help me please dear adventurs? My %PCP and %ASM are corrupted. AttachmentDesktop.zip (285 Downloads) |
8/15/2016 4:04 PM | |
Posts: 1 Rating: (0) |
Hi! It would be necessary to help! Sinumerik 810T PC software should be German, in English for now. Thanks!
|
8/17/2016 6:54 AM | |
Posts: 92 Rating: (5) |
Finaly I finish it My both 810T Works as well as and It was Unpossible Without Your Kindly Help. thank you , Mr Pee, Mr Nulizhng Mersi ( "mersi" is thank in my org language) I had [ PLC ALARM MESSEGE 6127 and ORD1 PLC STOP ], as you know it means is : " Selected interrupt input byte not available in hardware After error and trail I find its work in 15 and because i had new alarm 6104 ( Parameterization error in BMW or BDW command so I just chenge bit 0 to 1, in MD2002 . Orginaly it was : 10101000 and i chenge it to : 10101001 . Its work and my PLC STOP ALM cleard. I jast want to Know , Is it ok? Its work know but in future or in work it didnt make misstake? MD2002 Bit 0 is : [ No PLC alarm processing [ explanation PLC-MD 0
Attachment338_810_820_GA3_Installation_Instructions.pdf (352 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on