1/9/2016 3:33 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684)
|
Hello Dolpoong; Be aware that Step 7 Lite is a different product than Step 7 v5.5. First, Step 7 Lite stopped development under Win 2000 and Win XP Professional SP2; choose your OS accordingly: Which version of STEP 7 Lite is compatible with which version of MS Windows operating system and optional software package and which version of the Internet Explorer is required? https://support.industry.siemens.com/cs/cn/en/view/23642592
Step 7 Lite does not support any networking CPs or function modules, and the Information files accompanying the download should be checked to see if you can use the specific CPUs and IO modules you plan to work with. Also open the following FAQ: What are the essential differences between STEP 7 Lite and STEP 7 / STEP 7 Professional? https://support.industry.siemens.com/cs/ww/en/view/31031123
The file format of Step 7 Lite is different than standard Step 7; there is a procedure to migrate a Step 7 Lite to Step 7, but it is not automatic: How can you transfer a STEP 7 Lite user program to STEP 7 / STEP 7 Mini? https://support.industry.siemens.com/cs/ww/en/view/22586862
If you still intend to work with Step 7 Lite, for training purposes or single-machine programming, you would need the Step 7 Lite manual: Programming with STEP 7 Lite V3.0 https://support.industry.siemens.com/cs/cn/en/view/11441337 Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
Follow us on