8/16/2006 4:47 PM | |
Posts: 2 Rating: (0) |
Hi, How can I upgrade my S7 5.1 to 5.3? Thanks |
8/16/2006 4:53 PM | |
Joined: 4/24/2006 Last visit: 3/28/2024 Posts: 8610 Rating: (1144) |
Hello, You'll have to buy an upgrade to Step7 v5.3 6ES7810-4CC07-0YE5 http://support.automation.siemens.com/WW/view/en/18588571 But remember the actual version is Step7 v5.4 http://support.automation.siemens.com/WW/view/en/22445076 Best regards, Wizard |
8/16/2006 8:29 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
[quote user="CRI-Tech"]How can I upgrade my S7 5.1 to 5.3? Hi, Like Wizard says please upgrade for the same price to STEP7 V5.4 [;)] Then you are directly up-to-date for all new cards and functions, see the upgrade FAQ of V5.4. STEP 7 V5.4 Released for Delivery Please look also for the to use Windows Version... [:blush:] Which SIMATIC software packages are compatible with which Microsoft Windows operating system and with STEP 7 V5.4? |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
8/17/2006 8:01 PM | |
Posts: 2 Rating: (0) |
I have a new machine coming in to my area.The programmer wrote it with Step7 5.3 will I need 5.3 or higher to edit this program? |
8/17/2006 9:03 PM | |
Joined: 9/23/2005 Last visit: 3/11/2024 Posts: 4325 Rating: (1416) |
Yes |
Denilson Pegaia |
|
Follow us on