10/22/2014 6:14 PM | |
Posts: 20 Rating: (0) |
Thanks for the input. However, how do I get the actual tool number instead of the internal tool number?
|
10/24/2014 7:17 PM | |
Posts: 297 Rating: (41) |
If you don't have it yet, you should get Doc on CD, or at least the Tool Management manual, which is available at http://support.automation.siemens.com/WW/view/en/64914223 I think your machine is a lathe. I only work on milling machines, but I think the concept is the same, just your tools never leave the magazine. You should be able to use the $MYMLN function to get the location of a tool. So, $MYMLN[$P_TOOLNO] should return the magazine location of the current tool. HTH, SteveA |
This contribution was helpful to1 thankful Users |
Follow us on