3/21/2019 2:36 AM | |
Joined: 7/16/2015 Last visit: 8/20/2024 Posts: 8 Rating: (0) |
Dear, Pierre Could you solve the problem? Currently we have a problem with commissioning an Axis, Don´t finish the tuning and show the message. THE AMPLITUD OF THE MEASURED FRF CONTAINS EXCESSIVE FLUCTUATIONS Those problem appear when we commissioning the second system "line scale" of measure and try to perform the tuning. the axis move on auto and MDA without problem with the second system of measure but if we push JOG the axis move alone slowly without push + or - key Those efect don´t happend if we test only with the first system of measure. Best regard Javiersigrama ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/21/2019 12:55:33 PMNew subject after splitting |
|
3/21/2019 2:42 AM | |
Joined: 7/16/2015 Last visit: 8/20/2024 Posts: 8 Rating: (0) |
Hi, Can you give me suggestions? Best regards javiersigrama |
3/21/2019 2:48 PM | |
Posts: 2964 Rating: (482)
|
Hello, Does the scale resolutions are entered properly ? Please check in the service display screen measuring system 1 motor feedback and measuring system 2 feedback are matching properly ? is there is any deviation and following error are more? normally i suspect any one of this 2 could be problem.
|
Follow us on