10/3/2021 7:50 PM | |
Joined: 2/15/2021 Last visit: 4/14/2022 Posts: 14 Rating: (0) |
Hi, I have built a controller for my home made hot tub that controls temperature, drain pump, and in the future also opening of the pool cover. So far so good. 1. But to track the power consumption a bit from the heater I want to measure the time that the heater (Q1) has been on. In the attached program, all works fine in simulation. The temperature going lower than the set temp and the heater is starting. The counter adds 1 "switch on" and starts to count the time. This shows on the display and also in the diagram. But when downloaded, it does not work. I do not get the time to start counting and showing on the display and also, of course, not on the web interface. Any ideas about what I have done wrong? AttachmentPoolstyrning_V2.1.zip (333 Downloads) |
10/3/2021 7:54 PM | |
Joined: 12/18/2014 Last visit: 5/10/2024 Posts: 32996 Rating: (4078)
|
What do you mean with web interface? Mean you the extended webserver, programmed with the LWE? |
10/3/2021 8:56 PM | |
Joined: 12/18/2014 Last visit: 5/10/2024 Posts: 32996 Rating: (4078)
|
Can you please upload your LOGO! program and the LWE project as a ZIP file? |
10/3/2021 10:17 PM | |
Joined: 12/18/2014 Last visit: 5/10/2024 Posts: 32996 Rating: (4078)
|
Your LSC diagram is damaged. Try this ... AttachmentPoolstyrning_V2.2.zip (372 Downloads) |
10/4/2021 11:01 PM | |
Joined: 2/15/2021 Last visit: 4/14/2022 Posts: 14 Rating: (0) |
Hi, Here is both the program and the LWE project. I tried your 2.2 version and then there was still no time counting and the second temperature sensor just showed "-50" on the webpage. AttachmentPoolstyrning_V2.1.zip (339 Downloads) |
10/5/2021 4:15 AM | |
Joined: 12/18/2014 Last visit: 5/10/2024 Posts: 32996 Rating: (4078)
|
I controlled my V2.2, there a wrong selected parameter in Parameter-VM-Mapping of the Lufttemperatur. And I've forget to mapping the hours counter. Sorry. Here are the corrected versions. AttachmentPool.zip (348 Downloads) |
Follow us on