7/13/2016 11:00 PM | |
Posts: 1 Rating: (0) |
Hello, I just read your post from here: https://support.industry.siemens.com/tf/ww/en/posts/modbus-rtu-status-7000/147378/?page=0&pageSize=10 I have an S7-1515-2 PN with a RS232 PTP HF module acting as a slave. Under my instruction sets, I only have the Modbus (RTU) instruction set. I'm having similar issues where the COMM_LOAD will not output done, and the status stays 16#7000. I also never see the TX or RX lights blink on the front display. Thanks, Drew ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_958102 at: 7/13/2016 11:01:30 PMLast edited by: Min_Moderator at: 7/14/2016 10:41:27 AMNew subject after splitting |
|
7/14/2016 9:07 AM | |
Posts: 5225 Rating: (1192) |
Hi Duris_I. Added to your thoughts.. Thanks for helping! w |
This contribution was helpful to1 thankful Users |
Follow us on