3/25/2017 10:43 AM | |
Joined: 4/11/2014 Last visit: 9/13/2021 Posts: 22 Rating:
|
Hello Everyone. I have the same Issue in Wincc7.3 but its litte different from others. I have configured alarms from PLC and also some internal Tags.When the Alarm Bit Triggers,Actually the alarms displaying in Alarm control Window. But the COrresponding Text entered in Alarm configuration is not displaying.I mean the User Text Blocks like 1,2 from Alarm logging. But When i create a new project and try to repeat the Procedure,It was working Perfectly.But not with the old project BAckup. Right now the Problem is I need to solve this issue with the existing backup itself. I cannot Create new backup and copy the Pdl files into new backup. I have attached screenshot for this issue.Please anyone help me with this.. Thanks.. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/27/2017 4:04:20 PMNew subject after splitting |
|
Follow us on