1/1/2020 2:43 PM | |
Joined: 9/10/2019 Last visit: 10/12/2023 Posts: 30 Rating: (0) |
Hello, I have step7 project. I opened simatic v5.6 but my project has rexroth drive. I can not see rexroth drive. I setup drive es but this package dont have rexroth drive. Can you inform me? Thansk ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/02/2020 11:11:55New subject after splitting |
|
1/2/2020 5:33 PM | |
Joined: 9/27/2006 Last visit: 9/24/2024 Posts: 12282 Rating: (2685) |
Hello EngineerMan; You have been told already that you cannot integrate a 3rd-party drive in DriveES. If you have the gsd file for the drive you will purchase then you can insert the drive as a Profibus slave in the Profibus configurator of your S7 CPU. I have located a manual (rather old) for the HNC100 drive from Rexroth, the screenshot below describes how the drive is to be controlled by a S7 Profibus-DP master, through the gsd file first, then with specialized functions provided by Rexroth on an accompanying diskette (did I mention the document was rather old?). http://fs1.gongyeku.com/data/usershare/2015-8/20150828051042.pdf I suggest you determine which model of Rexroth drive you will purchase, and then contact Bosch Rexroth to obtain the gsd file, software support and documentation you will need for this project. And tell Rexroth what Siemens softwre you will use to control these drives, Simatic Manager and TIA Portal programs are incompatible. Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
1/2/2020 9:33 PM | |
Joined: 9/10/2019 Last visit: 10/12/2023 Posts: 30 Rating: (0) |
Hello dchartier, Thank you for helping. I will try it.
|
Follow us on