7/25/2017 9:54 AM | |
Posts: 4 Rating: (1) |
Hello, I am testing two Virtual Machines in VMWare, both of them with Windows Server 2012 R2 x64. You can see the installed software in the attached screens: 1. Information Server 2014 SP2 Update 3. 2. WinCC V7.4 + IS Ready 2014 SP2 Update 3. I have been able to add the WinCC project to Information Server, but when I try to create a report ("Table", in the image), the next error appears: "Configuration data cannot be retrieved from the selected project. Please try again in a few seconds. If the error persists, please check if the selected project (e.g. WinCC project) is up and running and if the ISReady on the OS machine is configured properly and is currently running". Futhermore, I have the WinCC project on runtime with different tags in Tag logging, with the Tag Simulator simulating them with random values. Finally, I have installed both system three times following the manuals with no result. Does anyone have any idea of what should I do? I have been in contact with Siemens support about this and they are not able to give me a solution. Thank you. Attachmentscreens.zip (246 Downloads) |
3/26/2020 6:06 AM | |
Joined: 10/29/2016 Last visit: 11/26/2021 Posts: 2 Rating: (0) |
Dear all, Greetings of the Day. i am also facing the same problem. kindly reply if any one have solution. |
7/24/2023 7:58 PM | |
Joined: 7/24/2023 Last visit: 7/24/2023 Posts: 1 Rating: (0) |
hola pudiste solucionar? en este momento tengo el mismo problema |
Follow us on