3/25/2020 7:20 PM | |
Joined: 4/13/2016 Last visit: 6/22/2022 Posts: 12 Rating: (0) |
Dear Georg, I have a some how same question in this regard. I am currently working on a plant which is not operational for 4 years almost. The installed WINCC Version is 7.3. Now , i want to install license key RT but the current license available version is for wincc v7.5 . can you kindly suggest me a step by step way? do i need to migrate the project from wincc v7.3 to wincc v7.5 (in this order i will need to install the software WINCC v7.5 to the stand alone wincc machine) to install the license keys or i can install on the same version. like WINCC v7.5 RT license on Current software with project on wincc(V7.3). Your earliest response will be highly appreciated. Regards,
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/26/2020 10:26:36New subject after splitting |
|
5/26/2020 8:06 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello K_k_2, then the problem is in the USB-Port or in the USB-Stick. In the past, with former versions of WinCC, we had have If the USB-Stick may be really defekt, you could contact see FAQ: https://support.industry.siemens.com/cs/ww/en/view/772175
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
6/1/2020 9:56 AM | |
Joined: 4/13/2016 Last visit: 6/22/2022 Posts: 12 Rating: (0) |
Dear George, Thanks for you continuous support. I have plugged the license key USB and its indicating that the license of Runtine+Configuration is OK (Refer attached Picture) but it is still running in DEMO mode indicating that the licenses A9WRT and A9WRC are missing. Kindly let me know if my license does not cover A9WRT & A9WRC ?? Because What i assume is : If it is detecting the license of WINCC RC (As mentioned in picture) then it should not require an additional license of A9WRT and A9WRC. Kindly support me in this manner, Thanks
|
Last edited by: K_k_2 at: 06/01/2020 10:00:38Last edited by: K_k_2 at: 06/01/2020 13:58:40 |
|
Follow us on