1/20/2018 9:49 AM | |
Joined: 3/14/2017 Last visit: 7/23/2024 Posts: 103 Rating:
|
hey all i have one question regarding with file transfer to HMI device how to transfer? with regards ted |
1/20/2018 9:55 AM | |
Posts: 8946 Rating:
|
Push the "Transfer" - Button. |
1/21/2018 2:38 AM | |
Joined: 10/25/2016 Last visit: 9/1/2022 Posts: 199 Rating:
|
Hi, Before the transfer you must fill these conditions : ·The configured device type is identical to that of the target device ·The configured device version matches that of the image (operating system) on the target device ·A connection has been established to the target device (transfer interface settings)·The target device is ready for transfer (transfer mode active) ( see panel setting attachment) ·The project can be generated without errors
Then you can transfer, Enjoy and be tenacious especially the first time Attachmentwincc.zip (398 Downloads) |
1/24/2018 6:00 AM | |
Joined: 3/14/2017 Last visit: 7/23/2024 Posts: 103 Rating:
|
thanks snoop for your post |
1/28/2018 6:19 PM | |
Joined: 10/25/2016 Last visit: 9/1/2022 Posts: 199 Rating:
|
|
This contribution was helpful to
1 thankful Users |
Follow us on