5/21/2012 9:21 PM | |
Posts: 621 Rating: (10) |
Hi Vithani Ayman Elotaify and friends as per you both suggeste me to check the P1080 = 0000 is there and P1082=5000 and r752 is also 00 so that Finally i was made second analog input scaling ie P0757=4.00 in index 0 and 1 the same ting in P0759=20.00 in index 0 and 1 now scale is measuring properly 4-20ma and disply showing 0-50Hz now working fine as per frequency set point and speed variation(speed rfeferance ) thank you very much for the good support you all regards algudkar |
This contribution was helpful to1 thankful Users |
5/21/2012 9:38 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477)
|
Hello Algudkar Its good that you got it working Just a thing, looks like problem was in AI scaling. But you said you checked by running from BOP too (P1000-1) Then AI scaling should not affect at that time You also wrote that you tried to scale Both index
I guess you were doing something wrong while checking all this |
Last edited by: Vithani at: 5/21/2012 9:39 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
5/22/2012 4:25 PM | |
Posts: 621 Rating: (10) |
Hi yes here only this i was didsomething wrong while im checking . regards algudkar |
Follow us on