7/9/2020 4:20 PM | |
Posts: 1 Rating: (0) |
I am woking with 1500R-2PN cpu (6ES7 515-2RM00-0AB0). For profinet port 2 X2 i am using class B ip address : 192.168.0.100, subnet mask:255.255.0.0. My ES/OS has ip address of same class : 192.168.1.150, subnet mask:255.255.0.0. In above scenario i am not able to ping the CPU https://snaptube.cam/. In my Architecture i am having TP900 comfort HMI with ip address : 192.168.0.150, subnet mask:255.255.0.0. which i can ping with my ES/OS 9apps. As per subnet mask i am using 255.255.0.0 allowed usable host IP address range are 192.168.0.1 - 192.168.255.254, so ideally PLC should ping the IP addresses i am using but in reality its not happening. Kindly advice for any 1500R setting is missing. which can help me to established the communication. |
Last edited by: Damiangage at: 07/12/2020 06:15:49 |
|
Follow us on