9/13/2019 1:09 PM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1643)
|
Hello hmmm. I think you will not get a suitable information for this situation. I never tried such a big size of USB Pen. Siemens has always the statement that only the Siemens USB Sticks for the Panels are released and System tested for the HMI Panels (and this ones are not as big). So they will also give you no Go. I think you can only try it or use a network share for this topic. Let the Panel store the Log files to a network share and then you will not have this problem: https://support.industry.siemens.com/cs/ww/en/view/92346478 But be careful with the maximum size of the Logfiles, a TP 700 Comfort should not have more that 20000 entries in one archive. If you need more then you can use long time archiving: https://support.industry.siemens.com/cs/de/en/view/109477071 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on