7/1/2020 8:20 AM | |
Joined: 12/28/2016 Last visit: 4/20/2024 Posts: 429 Rating: (44) |
Hello I want to migrate a project from wincc 7.0 to wincc 7.5 The problem is that after migrating to the new version, some objects do not work properly, for example, the color of some objects does not change properly, or some objects are displayed with a long delay. I first migrated the project from wincc 7.0 to wincc 7.2 and then from 7.2 to 7.5 Sp1. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/01/2020 11:18:26New subject after splitting https://pnap.ir |
|
7/1/2020 8:44 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Madadi, if you have installed WinCC V7.5 SP1 without Updates, https://support.industry.siemens.com/cs/de/en/view/109773812 Futhermore you short execute the "Convert Project Data"
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
7/1/2020 11:11 AM | |
Joined: 12/28/2016 Last visit: 4/20/2024 Posts: 429 Rating: (44) |
thanks for your response I tested the project with wincc 7.5 without SP1 It looks good in Simulation, but needs to be tested with a CPU I'm also installing an update to test with wincc 7.5 sp1 |
https://pnap.ir |
|
7/1/2020 12:08 PM | |
Joined: 12/28/2016 Last visit: 4/20/2024 Posts: 429 Rating: (44) |
After updating and testing with Simulink, the problem seems to be solved. But it is necessary to check at the project site. Thanks
|
https://pnap.ir |
|
Follow us on