6/26/2013 12:35 PM | |
Posts: 1 Rating: (0) |
Hay Devesh, to use analog i/p as freq. set point, what to set for P700? 0 or 2? and how to define On / Off and direction change by DIPs? Regards |
Last edited by: CS Moderator at: 6/29/2013 11:56 PMnew subject after splitting from /tf/WW/en/Posts/91528#top |
|
6/26/2013 5:42 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
P700 - is source of Control - means start or stop - you should set 1 if you want to start it using BOP or set to 2 if you want to start using Terminals (DI) For Setpoint - you should set P1000 - for analog set 2, for BOP set 1 For On-off using DIs, you have to set 1 in that particular input For DI1- set P701 to 1, for DI2- set P702 and so on Now for direction reverse, if you want particular input as start and other is for Reverse you should use P1113 For example, when DI1 is ON, drive ON - P701 = 1, now you get DI2 and drive will change direction -P702 = 99 and P1113=722.1 If you want DI1- Drive ON forward and DI2- Drive on Reverse P701-1 P702-2 you can study Manual - Operating Instruction and Parameter List for More help Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on