7/18/2019 9:23 AM | |
Joined: 10/27/2009 Last visit: 3/15/2024 Posts: 455 Rating: (77) |
Probably You try to program the spindle axis in coordination with a linear axis like that: N10 M3 S50 ; spind movement N15 M5 ; spind stop N20 M70 N30 G1 G94 F500 X100 C100 ; coordinated mvement with X-Axis Therefor You need to change the spindle in "axis mode". The command is "M70". ==> N20 The attached PDF shows all possible changes in between of the different modes of a spindle. If required the feedrate of such a combination is to be adjusted via FGROUP-command. (There was a corresponding thread here in the forum a couple of days before) AttachmentFunction Manual Basic Functions .pdf (61 Downloads) |
hope that helps |
|
Follow us on