7/28/2011 11:49 AM | |
Posts: 10 Rating: (0) |
Dear All We have used PCS7.1 sp1 for our application. Last time my pc gets crashed and i have to install the win xp on my system again. So i do the fresh installation of pcs 7 agian on that PC. but now problem is that when i compile the chart then it shows error "S7 scl is not installed". But when i see in the add/removes program then it was there. Please see the attachec error screen shot. I have agin install the s7 scl component from pcs7 DVD.But the problem was remain there. Please help me to solve the issue. Thanks Kapil Attachmentcompilation error.zip (61 Downloads) |
7/29/2011 8:06 AM | |
Posts: 10 Rating: (0) |
Dear Phantom MyLaptop had crashed and i do the new winXP sp3 installation on this.Then I installed the PCS7.1 sp1 on my laptop but it takes 6-7 hours for installation.after that i made a new project using project wizard but it is not working ,laptop gets hanged. Then aftet thisi remove all component od PCS7 one by one from Add/remove program and do the installation of PCs 7 with new dump from DVD.this time it isinstalled in 3 hours and project was created with wizard sucessfully.But when i compile the CFC then it is showing error of S7 scl not installed.But it is installed (as shown in add/remove program) on my laptop.I think there may be problem in the installation of this compenent so i install the s7 component from setup of PCs7. But poblem was remain the same. please find the attached Citamis.str file of my installation.check it there is any problem. Thanks Kapil AttachmentCitamis.zip (38 Downloads) |
Follow us on