1/15/2007 2:11 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
· Ok, firstly check your products are compatible using this FAQ · Ensure that the Windows Firewall is disabled. · Ensure you are not logged onto a domain when installing. · If Hyperthreading is available then you should disable it in the BIOS · Disable / uninstall any anti-virus software while installing Salma |
1/15/2007 8:34 PM | |
Posts: 66 Rating: (1) |
· Ok, firstly check your products are compatible using this FAQ This should be OK Simatic S7 5.3 SP3 Simatic Net 2005 6.3 HF1 WinCC v6.0 HF2 · Ensure that the Windows Firewall is disabled. Yes · Ensure you are not logged onto a domain when installing. OK · If Hyperthreading is available then you should disable it in the BIOS Should be OK · Disable / uninstall any anti-virus software while installing Yes I have now uninstalled WinCC, message queing and MSSQL in addition I have deleted regisry entries for WinCC flexible, WinCC HMI and MSSQL. Any more registry items that would be smart to delete? Tomorrow I will install everything again according to the items in this post! Fingers crossed! V |
Last edited by: vidarv at: 1/15/2007 8:34 PM |
|
1/18/2007 2:08 PM | |
Posts: 1275 Rating: (123)
|
Hello V, The latest version of WinCC Flexible is 2005 SP1, you may find some info on setting up Flexible's system here. I would've installed Flexible before WinCC and it's components, as I said... did you create an image of a clean windows installation? Best regards, Danielle |
1/26/2007 9:18 AM | |
Posts: 66 Rating: (1) |
Hia Danielle! TY for your reply. Any news? |
2/2/2007 1:58 PM | |
Posts: 1275 Rating: (123)
|
Hi V, Here's what support sent us, they're working with the possibility of pcAnywhere disabling DCOM. That's not what happened in our case, since pcAnywhere had never been installed. Still, here it is, in case it may help you: Please check the following FAQ: >>http://support.automation.siemens.com/WW/view/en/16640039 The FAQ descibres the software pcAnywhere which disables the DCOM Interface. There are other software packages that disable the DCOM Interface aswell. Restart the PC, download the *.reg file and execute it. After this step WinCC should work again. Best regards, Danielle |
2/3/2007 7:25 PM | |
Posts: 66 Rating: (1) |
Hia Danielle! I had WinCC and PCanywhere running together without any problems. V |
Last edited by: vidarv at: 2/3/2007 7:26 PM |
|
2/4/2007 8:09 PM | |
Posts: 66 Rating: (1) |
Hia again! I have just read the support entry again: (http://support.automation.siemens.com/WW/view/en/16640039)Possible causes of the HResult error message:
This could verry well be what happend to me, I deinstalled PCAnywhere and the Regedit entry was removed! But for your problem Danielle this probably don't explain anything! Vidar |
2/6/2007 9:14 AM | |
Posts: 1776 Rating: (95)
|
Hi, have You tried Salma`s solution? Also check the FAQ http://support.automation.siemens.com/WW/view/de/22056585 April |
7/20/2013 11:20 AM | |
Posts: 691 Rating: (36) |
Are you using any anti-virus programs which are not approved by SIEMENS? Antiviruses |
Last edited by: Niranjan Prasad at: 7/20/2013 11:25 AM |
|
7/20/2013 11:38 AM | |
Joined: 10/31/2011 Last visit: 4/29/2024 Posts: 400 Rating: (5) |
DEAR PRASAD, No i hav't install any software even anti virus and pc hold fresh copy of windows.
|
7/31/2013 1:51 PM | |
Posts: 1776 Rating: (95)
|
Hi, maybe this links helps http://support.automation.siemens.com/WW/view/en/44443989 |
Follow us on