12/26/2015 3:35 PM | |
Joined: 3/30/2011 Last visit: 3/29/2024 Posts: 733 Rating: (255) |
Hello, I usually work with similar systems and I connect to drive with routing via plc. I use Scout instead of Starter but I think also with starter is the same. You can look here (it is for sinamics but for MM is the same). In the attachment the screen to configure access point (in scout clicking access point in accessible node windows). Best Regards |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
This contribution was helpful to1 thankful Users |
Follow us on