12/18/2007 10:17 AM | |
Posts: 1 Rating: (0) |
Please could you help me I have: V3.2 Step7 MicroWIN SP4 STEP 7-MicroWIN 32 Instruction Library ToolBox V1.0 STEP 7-MicroWIN 32 Instruction Library ToolBox V1.1 CPU 215-2 Profibus DP 6es7 215-28000-0xb0 and Micromaster Vector 6SE3212-1CA40 I am truing to teach my self how to control Invertot from CPUs inputs. I made simple program - using USS_Init and USS_CTRL but when i an truin to compile it, debugger window shows me 111 errors - most of them are - The instruction is not supported by PLC type selected Parametrized subroutines are not supported by PLC type selected, Memory area is not valid for the instruction operand Also i dont understand why last error appears - i have defined library memory allocation from VB100 through VB496. Please could you help me or give an advise how to correct the situation. I am including my project file in the topic. Sorry for my bad english. AttachmentProject2.zip (212 Downloads) |
1/8/2008 10:33 AM | |
Posts: 739 Rating: (55)
|
Hello, Please find attached a couple of FAQ which may help. http://support.automation.siemens.com/WW/view/en/5734889 http://support.automation.siemens.com/WW/view/en/2360871 http://support.automation.siemens.com/WW/view/en/2409301 ----------------------------------------------------------------------------------- For more technical consulting please contact the Technical Support for Automation & Drives SIEMENS AG Tel: +49 (0) 180 5050 222 Fax: +49 (0) 180 5050 223 Mail: adsupport@siemens.com Support Request: http://www.siemens.com/automation/support-request Internet: http://www.siemens.com/automation/service&support FAQ : http://www.siemens.com/automation/csi_en/product |
1/8/2008 8:12 PM | |
Posts: 130 Rating: (1) |
ifsla6ku: I opened your project and the errors listed are: USS8 (INT2) Network 6. line 1. ERROR 11: The instruction is not supported by the PLC type selected. Network 8. line 1. ERROR 11: The instruction is not supported by the PLC type selected. Network 14, line 1. ERROR 11: The instruction is not supported by the PLC type selected. Network 14, line 2. ERROR 11: The instruction is not supported by the PLC type selected. Network 25. line 1, ERROR 11: The instruction is not supported by the PLC type selected. USS9 (INT3) Block Size = 0 (bytes). 106 errors This indicates the cpu does not support an instruction I don't believe you can communicate USS with the s7-215dp. The S7-215dp isa profibus slave, and does not have a freeport mode and therefore cannot communicate USS. You might refer the link below. http://support.automation.siemens.com/WW/view/en/733797 Also the product manual section 9.1 addresses the communication possibilities. I changed your processor to a 224 and it compiled w/o any other changes JensScorrect me if i am wrong please, i looked at your links and they didn't seem to match what i interpreted. AttachmentProject2_224.zip (224 Downloads) |
Follow us on