1/9/2014 8:08 PM | |
Posts: 3 Rating: (0) |
Hello I have one question How can i control mm440 with serial (RS485) port ?
|
1/9/2014 11:33 PM | |||
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello kamyar; What serial port do you mean? You can use the USS protocol to control a Siemens drive over RS-485 (you can also use Profibus-DP, which uses RS-485 also, but then you need a processor for your MM4 drive). Here are the specifictions of the USS protocol: Specification: Universal Serial Interface Protocol USS Protocol Do you plan on controlling the drive froma PC, a PLC? The only implementation of the USS protocol on a PCthat I know of is part of the SimaticDrive ES package:
S7-200 PLCs can add a USS protocolMicrowin library (to be purchased) to control drives: The protocol functions are described here: S7-200 System Manual S7-1200 PLCs have an included USS library in Step 7 Basic, V. 11 and V. 12. For example, look in the following manual: On the S7-300 distributed IO (ET 200S) you can use a 1SI serial CP to use the USS protocol; you can dowload the library from the link in this FAQ: Hope this helps, Daniel Chartier |
||
Last edited by: dchartier at: 1/10/2014 2:25 PMLast edited by: dchartier at: 1/9/2014 11:37 PM |
|||
This contribution was helpful to1 thankful Users |
Follow us on