8/14/2008 11:31 AM | |
Posts: 1 Rating: (0) |
I have attached the engineering calculation details of the elevator for your reference i have used SLVC (P1300=20) as the control mode & have followed the procedure as mentioned in the FAQ of siemens support website. I have attached details of the same. i have used the following parameters & the values related to this control mode. P0625=33.5 P1472=35 P1496=100 P1511=2890 P0342=9 P2890=100.5 P1470=21 P1520=200.06 P1521= -200.06 P1610=200 P1611=100 P1745=5 P1755=4.8 P1310=100 P1311=0 P1312=0 P1215=1 P1216=1.7 P1217=1.7 P1236=0 P1237=4 P1240=0 P0346=2 P0344=120 P0701=0 P0702=0 P0731=52.D P0732=52.C P0733=0 P0601=1 After motor data identification P1910 = 1 & 3 , parameter r1787=0 the drive is operated by PLC on profibus. i have used a positive setpoint for hoisting the counterweight & negative setpoint to lower it. With these parameter settings,the motor drives the counterweight making a vibration sound. the motor doesnt operate smoothly. when the counterweight comes down the motor makes a light vibrating sound.If i try to optimise the parameters more,the operation becomes instable.the counterweight rolls back slowly when the command to hoist is given. i tried the flux current control method (P1300=1). But am not able to hold the counterweight i would like to know the following. 1) Is the motor selected suitable to hoist & lower the load? If not,what would be the suitable motor? 2) If the selected motor is suitable,then what would be the parameters i need to optimise? Or will any other control mode be suitable to make this lift work? please advise. If required any other details please let me know or mail me to jeevanmark@gmail.com Attachment2103.zip (176 Downloads) |
8/14/2008 12:13 PM | |
Posts: 29 Rating: (1) |
Hello, take a look at these links: http://support.automation.siemens.com/WW/view/en/20285941 and http://support.automation.siemens.com/WW/view/eb/22318072 Perhaps they can help you. Regards |
Follow us on