12/28/2018 3:18 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Hi all, I am facing a problem in configuring the IP address in X5 and X8 port. The detail as below Rack 0 X5- 10.50.251.11 , 255.255.0.0 X8- 10.50.225.11 , 255.255.255.0 Rack 1 X5- 10.50.252.12 , 255.255.0.0 X8- 10.50.225.12 , 255.255.255.0 Compilation no error, however when I download, the CPU indicates “inconsistent configuration/specification of the IP address”. Details of diagnostics is “An IP address which is in the same subnet as the IP address of this interface has already been configured/assigned for another interface. “ I do not know what the relationship between X5 and X8 port is. Is it a switch? If I assign X8 port subnet to 255.255.0.0, it prompted an error, said:" The subnet addresses of the two IO controllers 'CPU-01-X5' and 'CPU-01-X8' must not be the same." Can anyone help me to solve this? Thank you~ |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on