9/19/2020 8:59 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Shezerso; When you say you wish to access the ET 200S webserver (to simulate it) do you mean you are using a IM 151-8 CPU, on the ET 200S station? If this is the case, you might be interested in this section of the IM 151-8 manual, discussing the webserver, what can be accessed on the cPU and what interfaces are available: https://support.industry.siemens.com/cs/ww/en/view/47409312/21405912843 Hope this helps, Daniel Chartier |
9/19/2020 9:07 PM | |
Posts: 7 Rating: (0) |
Not exactly! I don't have the PLC with me right now, so the idea is, try to simulate the PLC via localhost (PLCSIM didn't work) and then, acess the webserver from this localhost PLC. |
Follow us on